Cancel
Showing results for 
Search instead for 
Did you mean: 

Re-size base planes in Sync

PLM World Member Pioneer PLM World Member Pioneer
PLM World Member Pioneer

Is it possible to re-size a base reference plan in sync mode in part?  I have to switch to ordered to get a the dynamic edit command, re-size and then switch back to sync.

Thak you for your help.

 

ST8  MP3

3 REPLIES

Re: Re-size base planes in Sync

Phenom
Phenom

Hi,

 

the only way that I know is through editing of Solid Edge Options, so you can change globally the plane size of 120,00mm to your desired value.

 

But I have to say, that Solid Edge make it accessible/possible -in Synchronous Mode too- to choose the commande "Dynamic Edition" of reference planes, but it's not active.It shoud be better that Solid Edge desable all them that are not accessible in one of the modes.

 

Yasser

 

dynamic_edition_01.jpgdynamic_edition_02.jpg

Re: Re-size base planes in Sync

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That still doesn't explain why you can't edit default reference planes directly as you can in ordered. Additionally by these option settings the plane is equal in X and Y unlike the ability in ordered to change one axis.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Re-size base planes in Sync

Honored Contributor
Honored Contributor

Yet another reason I avoid Sync.