Cancel
Showing results for 
Search instead for 
Did you mean: 

Ready only status

Experimenter
Experimenter

Hi,

 

At this moment we use a network drive as working directory for the development of a machine. 

This means that all the neccesary files are in 1 folder and a number of engineers are constantly editing these files.

 

Sometimes it happens that an engineer has opened a read-only file because its in use by an other engineer. Is it possible to see wich engineer has opened the original file? 

 

A bit like in Microsoft Excel, where you can see wich user opened the original file.

5 REPLIES 5

Re: Ready only status

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If the Read Only Assistant (click button in upper right of graphics screen) doesn't show you, then No.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Ready only status

Siemens Phenom Siemens Phenom
Siemens Phenom

From within Solid Edge, other than what Ken has mentioned, there is no way to tell who has a file lock.

 

If you can access the file server, the file server can tell you who has the lock.  If direct file server access is not possible, there are plenty of third party tools available to allow you to query who has a lock on a file. 

 

Or you could implement a PLM solution ;-)

Re: Ready only status

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"Or you could implement a PLM solution ;-)"

 

That will fix all his problems won't it Dave Man Tongue



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Ready only status

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you're including Insight in "PLM" then yes, you can see the user in the status indicator.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Ready only status

Builder
Builder

No PLM required for ST9 just use built in data manager.  Utilize the file status and display it in pathfinder.  It will report in use by etc.......

 

Phil

ST9
WIN 7Pro 64bit
DELL T5810 3.7-4Ghz 32Gb ECC