Cancel
Showing results for 
Search instead for 
Did you mean: 

Rectangular and Circular Patterns in Sketches

Experimenter
Experimenter

Is there a way to created associative circular or rectangular sketch patterns in Solid Edge ST8 (Ordered and Synchronous modes)?  I could only see the pattern function for sketches in the Ordered mode and it only put dots at the locations, it did not allow copying of sketch entities!?!  AutoCAD and SolidWorks allow patterning of sketch entities.  Doesn't Solid Edge allow this?

3 REPLIES 3

Re: Rectangular and Circular Patterns in Sketches

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Re: Rectangular and Circular Patterns in Sketches

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Just wondering if you have another link to see how to do it ?

 

I want to pattern some objects in Sketch environment but without results.

 

This function is the weirdest one I have worked with.

(view in My Videos)

 

Thank you.

 

Arek

 

 

Re: Rectangular and Circular Patterns in Sketches

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The short answer is you can't pattern sketch entities within the pattern sketch. But can pattern that sketch. So you need a separate sketch which patterns that sketch with the "roo".

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200