Cancel
Showing results for 
Search instead for 
Did you mean: 

Redo Inop

N/A

I started to do another doc and it would not redo... so I desided to close. I believe the doc is in another file which I could not open. And how to retrieve, send to another file. Same issue as last time
http://screencast.com/t/Axcqvap4
Thanks
Crousie

1 REPLY

Re: Redo Inop

Esteemed Contributor
Esteemed Contributor
The video shows you attempting to place a "feature" library item into an empty file. The intent of the Feature Library is that you are adding this to an EXISTING solid which you DO NOT HAVE.
If you want to start a new part from existing geometry you have 2 options...
Open the existing file and perform a Save As.
Create a new Part and use the Insert Part Copy command.
Be aware that utilizing the Insert Part Copy command will yield a solid with no features...


Ken

Production: ST10 MP5
Testing: SE 2019