Cancel
Showing results for 
Search instead for 
Did you mean: 

Referencing a variable in a custom property

Phenom
Phenom

Is it possible to build a custom property value from variables.

I want to reference the length, width and thickness variables for a part to build a property that reads Length x Width x Thickness.

I can then reference this in my parts list and add the size after the description.

I know that in a parts list I can refer directly to the variables, but some these are not applicable to all parts in the parts list, so I end up with "Description  x x".

We are using ST5.

Is there any difference in ST6?

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.
1 REPLY

Just click on the first blank line at the end of the vari...

Valued Contributor
Valued Contributor

Just click on the first blank line at the end of the variables table and type in the name. Then click in the "Formula" field and type "Length * Width * Thickness" and then click the Expose box to the right.

Terry Tyson
Software Automation Designer