Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Regarding Creating models in Synchronous Techonology

Pioneer
Pioneer

Hello

 

Can we use "Feature Library" use in Sheet metail & part solid model?

Also I required help files in pdf, regarding creating models in "Synchronous Techonology"

 

Thanks,

 

Somnath

21 REPLIES 21

Re: Regarding Creating models in Synchronous Techonology

Gears Phenom Gears Phenom
Gears Phenom

YES - Feature Library can be used in both Part and Sheetmetal environments. 

 

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Regarding Creating models in Synchronous Techonology

Pioneer
Pioneer
Is there any examples or video available?
Because I tried to cutout feature drag from feature library but not allowed to drop on tab in sheet metal.

Thanks.
Somnath

Re: Regarding Creating models in Synchronous Techonology

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Somnath_Pore

 

featuer library is working for Sync model too.

Just tested with cutouts from aprt and sheet metal files and added them into sheet metal parts and parts too.

 

 

regards
Wolfgang

Re: Regarding Creating models in Synchronous Techonology

Pioneer
Pioneer
Sir,
Can u Pl share me video file so I can try at my side...

Thanks
Somnath

Re: Regarding Creating models in Synchronous Techonology

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Somnath_Pore

 

 

even if not fully understanding the need for a video, since it should be explained enough within help pages
see the attached short vieo.

I am creating cutouts in sheet as well as in aprt files, save them in feature library and use them in every type of document again.

 

(view in My Videos)

regards
Wolfgang

Re: Regarding Creating models in Synchronous Techonology

Pioneer
Pioneer
Thank you sir!!

Re: Regarding Creating models in Synchronous Techonology

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Maybe this is the problem: The features have to be created in ordered or sync in order to work in ordered or sync. IOW you can't use an ordered feature when in sync mode and vice versa.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Regarding Creating models in Synchronous Techonology

Pioneer
Pioneer
OK..
I was using ordered part feature in sync
That's why it was not getting inserted in sync

Thanks
Somnath

Re: Regarding Creating models in Synchronous Techonology

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Bruce is a mind-reader.

You nailed it @bshand