Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Regarding making Cutouts & holes in frame designed contents

Pioneer
Pioneer

Dear sir,

 

is there possibility to make cutouts & holes in Frame Designed component like Square & round pipe

frame desgn.JPG

Regards,

 

Somnath

6 REPLIES 6

Re: Regarding making Cutouts & holes in frame designed contents

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Somnath_Pore,

 

Yes, as mentioned in your other post....using Assembly Features.......

 

2018-08-07.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Regarding making Cutouts & holes in frame designed contents

Pioneer
Pioneer

Pl. find my video recentely I created. cutout not generated.

 

(view in My Videos)

Re: Regarding making Cutouts & holes in frame designed contents

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Ahhh, OK.......your issue is the assembly feature [FOR FRAMES] must use the "Create Assembly Features" option, so that the parent part doesn't get modified.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Regarding making Cutouts & holes in frame designed contents

Pioneer
Pioneer

Thank You Very Much Sir!!Smiley Happy

Re: Regarding making Cutouts & holes in frame designed contents

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Somnath_Pore

 

 

You clearly can see it in Your video:

 

You have to create an Assembly Feature and not an Assembly Driven Feature!

 (First option instead of second one)

This is a big difference. 

First only exists in the assembly where else the second one only is defined in an assembly but should be stored back in the original part.

This will not work for Frame components.

 

Compare it with seeing a feature in the part / part drawing or not.

 

Such holes only exists in the assembly since the are created after welding the frame components.

regards
Wolfgang

Re: Regarding making Cutouts & holes in frame designed contents

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Very welcome. Robot Happy

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000