Cancel
Showing results for 
Search instead for 
Did you mean: 

Reinstall SolidEdge ST9 on a formatted PC

Experimenter
Experimenter

Hi guys,

 

Good day to you. Recently I just formated the Solid Edge computer with Windows 7 SP1 fresh installation. Now I want to reinstall back the Solid Edge ST9. How do I activate the license on that computer? 

 

I check my ex-colleague and she received one email with license key text file (SELicense.txt) but the setting inside the license key using "this_host"  so should I change it to the computer name (hostname)?

 

FYI I will install Solid Edge ST9 into this new formatted computer.

 

Thanking you in advance. 

 

Regards,

AELUser

 

 

8 REPLIES

Betreff: Reinstall SolidEdge ST9 on a formatted PC

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


the info "this_host" within the license file seems for me to come from a floating license, which means that here should be a license server running from which You can get Your "ready to start" Solid Edge

 

Ask Your college what the name of the SE license server in the network is and then either change the place holder "this_host" to the license server name or start the lciense wizzart from the start menü and there You choose license server and give there the name of it.

 

A floating license normally doesn't conflict with Your PC reinstallation

 

regards
Wolfgang

Betreff: Reinstall SolidEdge ST9 on a formatted PC

Experimenter
Experimenter

Dear Sir,

 

Sorry for the reply. Now I done most of the setup already which I refering from Internet. But when I going to start the Flexnet license Manager I encounter problem to start the service from LMTOOLS utility.

 

I alway get the error nessage :  VD is starting. Please check vendor daemon's status in debug log.

 

I seems got difficulty to start my services on FLEXlm license manager

 

My debug log message is following :

--------------------------------------------------------------------------------------------------------------------------------

3:47:31 (lmgrd) Server's System Date and Time: Wed Sep 21 2016 13:47:31 Malay Peninsula Standard Time
13:47:31 (lmgrd) pid 1748
13:47:31 (lmgrd) SLOG: Summary LOG statistics is enabled.
13:47:31 (lmgrd) Done rereading
13:47:31 (lmgrd) FlexNet Licensing (v11.13.1.3 build 176543 x64_n6) started on NCT-SIEMENS (IBM PC) (9/21/2016)
13:47:31 (lmgrd) Copyright (c) 1988-2015 Flexera Software LLC. All Rights Reserved.
13:47:31 (lmgrd) World Wide Web: http://www.flexerasoftware.com
13:47:31 (lmgrd) License file(s): C:\SEFlex\Program\SELicense.dat
13:47:31 (lmgrd) lmgrd tcp-port 27001
13:47:31 (lmgrd) (@lmgrd-SLOG@) ===============================================
13:47:31 (lmgrd) (@lmgrd-SLOG@) === LMGRD ===
13:47:31 (lmgrd) (@lmgrd-SLOG@) Start-Date: Wed Sep 21 2016 13:47:31 Malay Peninsula Standard Time
13:47:31 (lmgrd) (@lmgrd-SLOG@) PID: 1748
13:47:31 (lmgrd) (@lmgrd-SLOG@) LMGRD Version: v11.13.1.3 build 176543 x64_n6 ( build 176543 (ipv6))
13:47:31 (lmgrd) (@lmgrd-SLOG@)
13:47:31 (lmgrd) (@lmgrd-SLOG@) === Network Info ===
13:47:31 (lmgrd) (@lmgrd-SLOG@) Listening port: 27001
13:47:31 (lmgrd) (@lmgrd-SLOG@)
13:47:31 (lmgrd) (@lmgrd-SLOG@) === Startup Info ===
13:47:31 (lmgrd) (@lmgrd-SLOG@) Is LS run as a service: Yes
13:47:31 (lmgrd) (@lmgrd-SLOG@) Server Configuration: Single Server
13:47:31 (lmgrd) (@lmgrd-SLOG@) Command-line options used at LS startup: -c C:\SEFlex\Program\SELicense.dat -l C:\SEFlex\Program\Debug.log -z -s
13:47:31 (lmgrd) (@lmgrd-SLOG@) License file(s) used: C:\SEFlex\Program\SELicense.dat
13:47:31 (lmgrd) (@lmgrd-SLOG@) ===============================================
13:47:31 (lmgrd) SLOG: FNPLS-INTERNAL-VL1-4096
13:47:31 (lmgrd) Starting vendor daemons ...
13:47:31 (lmgrd) Started selmd (pid 2436)
13:47:36 (lmgrd) selmd exited with status 123 ()
13:47:36 (lmgrd) Since this is an unknown status, license server
13:47:36 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:47:36 (lmgrd) REStarted selmd (pid 1716)
13:47:41 (lmgrd) selmd exited with status 123 ()
13:47:41 (lmgrd) Since this is an unknown status, license server
13:47:41 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:47:41 (lmgrd) REStarted selmd (pid 1100)
13:47:46 (lmgrd) selmd exited with status 123 ()
13:47:46 (lmgrd) Since this is an unknown status, license server
13:47:46 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:47:46 (lmgrd) REStarted selmd (pid 1228)
13:47:51 (lmgrd) selmd exited with status 123 ()
13:47:51 (lmgrd) Since this is an unknown status, license server
13:47:51 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:47:51 (lmgrd) REStarted selmd (pid 1836)
13:47:56 (lmgrd) selmd exited with status 123 ()
13:47:56 (lmgrd) Since this is an unknown status, license server
13:47:56 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:47:56 (lmgrd) REStarted selmd (pid 1928)
13:48:01 (lmgrd) selmd exited with status 123 ()
13:48:01 (lmgrd) Since this is an unknown status, license server
13:48:01 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:48:01 (lmgrd) REStarted selmd (pid 2564)
13:48:06 (lmgrd) selmd exited with status 123 ()
13:48:06 (lmgrd) Since this is an unknown status, license server
13:48:06 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:48:06 (lmgrd) REStarted selmd (pid 1840)
13:48:11 (lmgrd) selmd exited with status 123 ()
13:48:11 (lmgrd) Since this is an unknown status, license server
13:48:11 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:48:11 (lmgrd) REStarted selmd (pid 2652)
13:48:16 (lmgrd) selmd exited with status 123 ()
13:48:16 (lmgrd) Since this is an unknown status, license server
13:48:16 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:48:16 (lmgrd) REStarted selmd (pid 2636)
13:48:21 (lmgrd) selmd exited with status 123 ()
13:48:21 (lmgrd) Since this is an unknown status, license server
13:48:21 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
13:48:21 (lmgrd) REStarted selmd (pid 2644)
13:48:26 (lmgrd) selmd exited with status 123 ()
13:48:26 (lmgrd) Please correct problem and restart daemons

Betreff: Reinstall SolidEdge ST9 on a formatted PC

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,



is Your PC the designated license server?

If not then You need not to install the flexlm software.

 

This only is necessary at the license server

 

And there YOu need to install the dongle (sentinel) driver and You have to iinsert the license server dongle into the PC

Execpt the server identification is done via CID or ethernet adapter number

But if this is the case then You have to get a new license file

regards
Wolfgang

Betreff: Reinstall SolidEdge ST9 on a formatted PC

Experimenter
Experimenter

Dear Sir,

 

Thank you for your swift response. Yes my PC actually is designate as license server.  BTW how to do "server identification is done via CID or ethernet adapter number"? I have no experience on install the floating license server for Solid Edge before.

 

Well, please see my error log 2 attached on more detail on my issue. Many thanks..

 

GOD Bless... :-)

Betreff: Reinstall SolidEdge ST9 on a formatted PC

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

have You had this PC running as license server before reinstalltion too?

And if Yes, is there an USB dongle pluged in?

 

Who has installed this computer for the first installtion?

 

Without knowing what Your license really is, wether it is the license server or not it becomes difficult to give You the correct answers.

What type of licsen do You have?

 

regards
Wolfgang

Betreff: Reinstall SolidEdge ST9 on a formatted PC

Experimenter
Experimenter

Hi,

 

Yes the PC use too be the server last time before format. The one install during very first time no longer with the company already.

 

As you can see the following I extracted from my license file SELICENSE.DAT :

My license is floating license.

----------------------------------------------------------------------------------------------------------------------

SERVER this_host SE_HWKEY_ID=36243 27001
VENDOR selmd
INCREMENT solidedgeclassic selmd 109.0 permanent 2 SUPERSEDE \
DUP_GROUP=UHD ISSUED=15-jul-2016 BORROW=4368 ck=174 SIGN="0730 \
FF59 8024 BCF8 E838 8F0B 0483 C5A5 A118 B8FC AAED C1CD B6F5 \
774D BB13 0F1D 08D7 AF22 D8AB 1A39 6404 ED98 ECE6 E070 BFDE \
0779 162C B43A 8D32 4D12"
FEATURE server_id selmd 109.0 permanent 1 VENDOR_STRING="1472401 - \
AEL Engineering Sdn." user_info=W9R22XN1QI ISSUER=SIEMENS \
ck=208 SIGN="10DA 5086 225D E6EF A491 A871 F0BD 8EF7 8CD5 3663 \
3E21 43A0 0AE5 BA71 AC8A 076B 4ABB F1D8 125E B61D 911C D50E \
A03A 3007 8281 C83E CBC6 BED7 73E9 C3C4"

 

 

################################################################################
# #
# SOFTWARE LICENSE TO FEATURE NAME CROSS REFERENCE #
# Version: 109 Created: 07-15-2016 14:18:40#
# AEL Engineering Sdn. Bhd. Sold-To/Install: 1472401 #
################################################################################

# LICENSE PRODUCT QTY DESCRIPTION QTY FEATURE NAME

# --------------- ----- -------------------- ----- ---------------------------
# SE290 2 SE Classic FL 2 solidedgeclassic

 

Betreff: Reinstall SolidEdge ST9 on a formatted PC

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,



OK, this is a floating license for a flexlm server usig a usb dongle for identification.

 

This means, that You have to have the server dongle available and at least the dongle driver installed - before pluging in the dongle.

Then You have to install the flexlm software but as I interpret You license file, there was a borrowing done before 15th of July

 

You should have an original license file which You can use for installation and usage.

 

And then You can use that server for any worksation to get appropriate licenses when starting Solid Edge

 

 

regards
Wolfgang

Betreff: Reinstall SolidEdge ST9 on a formatted PC

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Dear,

 

- Uninstall license manager.
- Delete winsock Registry (find "winsock" from regestry and Export & than afterDelete it from "Current Usesr").
- Restart PC.
- Reinstall license manager.

 

Regards,

irfan