Cancel
Showing results for 
Search instead for 
Did you mean: 

Relation to CG?

Honored Contributor
Honored Contributor

Is there any way to create relations to the center of gravity? The goal is to have lifting lugs always on the CG of the finished part?

6 REPLIES

Re: Relation to CG?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are variables of center of mass: CoMX, CoMY, CoMZ

Maybe you can figure a way to use them.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Relation to CG?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

You also can create a coordinate system regarding the CM position, it's a dynamic relation, so after that you can create a relation, not directly with the CG but with the coordinate system.

 

Regards

 

Steve

Steve Fealinx

Re: Relation to CG?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@abisse_steve wrote:

You also can create a coordinate system regarding the CM position, it's a dynamic relation, so after that you can create a relation, not directly with the CG but with the coordinate system.

 

Regards

 

Steve


@abisse_steve, could you explain or demonstrate how you constrain a coordinate system to the CG? I can't get the new coordinate system to "stick" to the CG.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Relation to CG?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

 

 

(view in My Videos)

Steve Fealinx

Re: Relation to CG?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK. It only works in ordered.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Relation to CG?

Honored Contributor
Honored Contributor

I run into stuff like that frequently and is why I stay in ordered. Thanks for the solution!