Cancel
Showing results for 
Search instead for 
Did you mean: 

Relocate origin

Experimenter
Experimenter

Dear users,

 

I have recently created an assembled model in my Solid Edge program and now I am going to create a technical drawing using this model as a base. However, assembling the model I must have done some easy mistake not placing the base of the model straight into the coordinate system, so now it is tilting and doesn't lie paralell or orthagonal do the coordinate systems axes. This makes my Top-Left-Right-views in the technical drawing to look 3-dimensional instead of 2-dimensional as they should be.

 

Is there any way to change the place of origo and by that straighten up the technical drawing, maintaining the relationship between the assembled bodies and an explosion view I have created? Previous help texts regarding this matter give me errors and isn't possible due to the destroyed relationship. They also seem to be more focused on moving the actual model instead of the origin.

 

Thanks for any help,

 

Have a nice day,

Carl

3 REPLIES 3
Highlighted

Betreff: Relocate origin

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

try to go to the "Properties of Instances" (RMB on Top entry of pathfinder

 

You should see, that the first object is fixed and the orientation must be changeable.

You might change the x,y,z coordinates and axis angle of them

 

If all further parts are connected only to the first master part this change should show an appropriate result in main views

 

 

 

regards
Wolfgang

Re: Relocate origin

Genius
Genius

You could also use "Section" in the model, and turn it on or off, if working with the 2D view doesn't work out.

Re: Relocate origin

Phenom
Phenom

Hi Carl,

 

I would use the steering wheel to reposition parts like shown in this demonstration of EdgePLM

 

https://www.youtube.com/watch?v=pcQ6WR-A3QE

 

Yasser