Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Remote install of maintenance pack

I have a cmd script that will install ST10 (I have 30+ installs to do)

MSIEXEC /i "\\path on server\Solid Edge\Solid Edge ST10.msi" MYTEMPLATE=1 USERFILESPECXML="\\Path\ST10\WUK Options ST10.xml" USERFILESPEC="\\Path\ST10\SELicense.dat" SETPDMCLIENT=1 INSTALLDIR="C:\Program Files\Solid Edge ST10" /qb+ /l*v "C:\temp\mysilentsetup.log"

 

Which works well,

I also want to install the latest maintenance pack which is also on the server

I’v tried

"\\ path on server \”Solid_Edge_MSI_MP8.exe /s /v” /qn /l*v %temp%\mysilentupdateMP.log”

 

But it just ignores it

Iv also tried putting the MP in the installation update folder but cat get that to work either.

 

Any suggestions?

3 REPLIES

Re: Remote install of maintenance pack

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@stephen_gardner  I used your command string to install MP8 from my file server on my client machine using a CMD window opened as Administrator and it worked perfectly.  I assume you are also running this as Administrator?



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: Remote install of maintenance pack

Siemens Phenom Siemens Phenom
Siemens Phenom

Unless I am looking at it incorrectly, your syntax is wrong for maintenance pack install -- you have double quotes all in the wrong places…


As written you have this:

 

"G:\Software\Solid Edge\ST10\MP\1100008004\"Solid_Edge_MSI_MP8.exe /s /v" /qn /l*v %temp%\mysilentupdateMP.log"

 

You need this:

 

"G:\Software\Solid Edge\ST10\MP\1100008004\Solid_Edge_MSI_MP8.exe" /s /v" /qn /l*v %temp%\mysilentupdateMP.log"

 

Note the " before Solid_Edge_MSI_MP8.exe in your string -- it should be after not before this.

Re: Remote install of maintenance pack

Hi thanks

 

uk_dave I did try with the quotes in various places, should of mentioned that really, it seemed to think about it for a minutes or two then just end.

 

I found this to be a working solution:

start  /D"\\server\Software\SE ST10 64 E\Maintenance Packs\" /wait Solid_Edge_MSI_MP8.exe /i