Cancel
Showing results for 
Search instead for 
Did you mean: 

Removal of units when exposing variables!

Creator
Creator

hi dear collegues

I would like to ask  about how to make a text remove feature, but I want the text to be written in mirrored way

and I didn't find the way to do it in solid edge

as SolidWorks user, the option is there in SolidWorks you have the icon if you want the text to be written the normal way and another icon to write in a mirrored way, 

what about solidege

thanks in advance

Omar

5 REPLIES 5

Re: Removal of units when exposing variables!

Phenom
Phenom

Hi Omar,

 

if I understand you well you are looking for Removing the Units when exposing variables!

 

You can do it in 2 ways:

 

1-Solid Edge Options (In your Draft)
Uncheck  the box for showing Units

 

2-

In the Legend Option after: /CP or /GP… you have to add:
/NU
I think, It's for "No Units"

 

And it should work Smiley Happy

 

Yasser

 

NU_1.jpgNU_2.jpgNU_3.jpg

Re: Removal of units when exposing variables!

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @omarkadd

 


@omarkadd wrote:

I would like to ask  about how to make a text remove feature,


This suggests you want to cut out the text profile in Part with mirrored text.

Don't try to mirror the text profile

Create the cutout and mirror the feature.

 

What problems are you facing ? 

 

Do you want the mirror in Part or Draft ?

 

Also agreed that SW can flip text but it's just that. Same as what SE can do.

Neither can really mirror text like what the MirrText system variable of ACAD can accomplish.

Re: Removal of units when exposing variables!

Creator
Creator

hi tushar,

thanks again

sean gave me a suggestion and it's working fine

it was about engraving text in a part (stamping the part) but the text must be written the mirrored way

and sean gave me the way in the synchronous mode

using the steering wheel 

so once again thank you

kindly 

omar

Re: Removal of units when exposing variables!

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@omarkadd

 

Your title says "removal of units for variables"

Your content is about "reversal of text"

First you sent me a PM for this.

When I suggested you to post it on the forum, you sent a PM to Sean

You did not even respond to Yasser's reply

OK so where is Sean's suggestion ?

Re: Removal of units when exposing variables!

Creator
Creator

hi Tushar

I'm sorry for the title it was a mistake and apologize for this,

I post it in the forum and I also sent a PM to sean I did both 

here is the link for sean answer

https://youtu.be/fvTR5owhzX0

best regards