Cancel
Showing results for 
Search instead for 
Did you mean: 

Removed Solid Edge and now Cannot Re-install.

N/A

I removed Solid edge ST5 to install ST4 and every time it still says that there is another version installed on my computer. I have checked the entire hard drive for any remaining files and cannot find any. Please Help!!

3 REPLIES

Re: Removed Solid Edge and now Cannot Re-install.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Look in the ST5 delivery folders for I believe "SptTools" and find the "SECleanUpAll.exe". Run this only after you have uninstalled SE and see if that fixes the issue.


Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: Removed Solid Edge and now Cannot Re-install.

N/A
There are no st5 files left on my computer. When I even tried to re run the st5 program to install that again and it still says that there is another version on the computer and it cannnot install.
Thank you I searched my harddrive and found the program still there ran it and going to restart now.. Thank YOU!

Re: Removed Solid Edge and now Cannot Re-install.

Siemens Phenom Siemens Phenom
Siemens Phenom
Here are the steps to manually uninstall and clean up any Solid Edge
installed software:
1. Uninstall the Solid Edge software using Add/Remove Programs.
2. Manually delete the Solid Edge program folders typically in
C:\Program Files and/or C:\Program Files (X86).
3. Manually delete the Solid Edge user preference folder
%APPDATA%\Unigraphics Solutions.
4. Manually clean up the registry by deleting any Solid Edge registries
in the following locations:
HKEY_CURRENT_USER\Software\Unigraphics Solutions
HKEY_LOCAL_MACHINE\Software\Unigraphics Solutions
HKEY_LOCAL_MACHINE\Software\Wow6432Node\Unigraphics Solutions
5. Reboot the workstation.
6. Attempt to reinstall the software again.

Regards,
-Dave

On 25/01/2013 17:19, djculver1s@semo.edu wrote:
>
> There are no st5 files left on my computer. When I even tried to re run
> the st5 program to install that again and it still says that there is
> another version on the computer and it cannnot install.
>
>