Cancel
Showing results for 
Search instead for 
Did you mean: 

Removing All Reference Files

Experimenter
Experimenter

Someone prior to myself loved reference files at my current employer (masters, Excel templates, etc). Over the years these have been copied, pasted, and looped. I would very much like to remove all reference files and pare my models down to one or two files. 

 

So my question is can I remove all reference files in some way that will not require me to draw my parts over from scratch?

 

I work on a team where only myself and a drafter touch these files. I've been pushing the drafter to make sure his documenation is clean and neat. It would be really hypocritical of me not to do the same, but I am struggling here.

 

reference.jpg

6 REPLIES

Re: Removing All Reference Files

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Excel links are typically to variable table, so breaking the link would simply be deleting the reference.  The current applied value will remain.

 

Part Copies can be broken by going into the file that the Part Copy is placed in, editing the Part Copy and unchecking the "Lint to File" or by converting the Part Copy feature to Synchronous as it will break the link.  Thje body will remain "as is".

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Removing All Reference Files

Gears Phenom Gears Phenom
Gears Phenom

dont forget to check the BINDER...  sometimes you will have files linked there...

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Removing All Reference Files

Legend
Legend
Save as parasolid, and open again... Convert to synchronous if needed..

Or if part or sheetmetal, insert copy, but break link on import.. convert to synchronous if needed..

Both methods will give a clean new "2017" copy of the part... without all the links and stuf from the past...

Second method also keeps internal face names the same, so you can replace the old parts in assys without problems..

Kind regards,


Jan Bos
Emmen, The Netherlands
User since V3.5 testing ST10

Re: Removing All Reference Files

Pioneer
Pioneer

Hello KennyG,

 

I'm in the part copy file and I want to break the links. I can't find the "Lint to File" or "Line to File" checkbox you are talking about. Do I click on something in the design tree? Do I right click on the part? 

 

Thank you

Re: Removing All Reference Files

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Edit the part copy definition, go to the parameters step, uncheck link to file.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Removing All Reference Files

Pioneer
Pioneer

Sorry, where is this paramters step you're talking about. Is that the variable table? I don't see the check box you're talking about