Rendern trouble with Parallel Desktop 10 and 11, Windows 10 , ST8 Education

Experimenter
Experimenter

Hello,

i have trouble withe a module.

The module is hidden when i doesn`t move it. I think it`s a image buildup problem from Directx or OpenGL.

Whats happening ? 

 

[URL=http://de.tinypic.com/r/30ng83p/9]View My Video[/URL]

 

greets 

7 REPLIES

Re: Rendern trouble with Parallel Desktop 10 and 11, Windows 10 , ST8 Education

Esteemed Contributor
Esteemed Contributor

Based on your title of the post, sounds like you are running this on Mac using "Parallels" to run a virtual session of Windows 10.

 

First of all, this solution is not supported so you should not expect it to work.

 

Second, ST8 did not support Windows 10 when released and requires a Maintenance Patch to fully support it and Windows 10 also required the November 2015 update.  Are you runnning the latest Solid Edge Maintenance Patch for ST8? 

 


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Rendern trouble with Parallel Desktop 10 and 11, Windows 10 , ST8 Education

Experimenter
Experimenter

Hi,

i use the last ST8 academic. Where can i show for the version number in Solid edge ? 

Re: Rendern trouble with Parallel Desktop 10 and 11, Windows 10 , ST8 Education

Esteemed Contributor
Esteemed Contributor

Help, About Solid Edge

2016-07-25_11-21-04.png


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Rendern trouble with Parallel Desktop 10 and 11, Windows 10 , ST8 Education

Valued Contributor
Valued Contributor

I ran into similar issues running Solid Edge ST8 using Parallels on a Mac. Solid Edge requires OpenGL v3.0 or higher. Parallels only supports OpenGL v2.1.

David McMahon
Solid Edge ST10, MP3
HP Z2 Mini, Windows 10

Re: Rendern trouble with Parallel Desktop 10 and 11, Windows 10 , ST8 Education

Esteemed Contributor
Esteemed Contributor

Hi there @jok3r,

 

Your easiest, and probably the only real method, is to run Solid Edge on a native Windows setup.....all else seems a great effort, for a substandard, or failed, result.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Rendern trouble with Parallel Desktop 10 and 11, Windows 10 , ST8 Education

Experimenter
Experimenter

hi there

had same problem here.

solved as following [1]:

1. open new part

2. go to settings \ options

3. view

4. application display

5. choose software dependent

6. apply

7. restart solid edge

 

[1]: note: i use the german edition. so i am not sure if the translation is correct.

 

webadress for german help:

https://docs.plm.automation.siemens.com/tdoc/se/110/se_help#uid:xid1129777:xid1325275:index_visualiz...Smiley Surprised

 

 

 

my system configuration:

Apple MacBook Pro mid 2012 13" inch

2.9 GHz Intel Core i7 | 8 GB RAM | Intel HD Graphics 4000 512 MB

OS X 10.8.5 | Parallels Desktop 10 (Version 10.4.0) | Windows 7 Professional SP1

SolidEdge ST10 Academic, version 110.00.00.107 x64

Re: Rendern trouble with Parallel Desktop 10 and 11, Windows 10 , ST8 Education

Esteemed Contributor
Esteemed Contributor

@DaffyDuck  That will resolve the problem but it will also eliminate any hardware acceleration and effects provided by the graphics card.  This is the slowest graphics option, but without hardware support it is the only solution.

 

Still doesn't solve the issue of ST8 being ran on Windows 10 by the original poster, but I see you are running ST10 on Win 7 which is supported (just not on Parrallels Smiley Happy )...


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3