Reorder features in assembly?

Experimenter
Experimenter

I need to create a new assembly feature before the first feature in an assembly.

Or reorder assembly features in pathfinder.

Is this possible?

 

We don't use synchronous in our office and don't want to know how wonderful it is for this.

4 REPLIES

Re: Reorder features in assembly?

Esteemed Contributor
Esteemed Contributor

Synchronous doesn't apply to assemblies but I'm going to say that no, you can't reorder assembly features, nor can you add a feature before the first. Before the second, yes, as I'm guessing you already know.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Reorder features in assembly?

you can use the GOTO command within Assy Feature collector in the PF...  

 

But you can not reorder... 

 

Assy Features are only Ordered and act as such

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6

Re: Reorder features in assembly?

Experimenter
Experimenter
Thanks bshand.
No, I didn't know I could reorder before the second.
How do I do that?
I've tried click and drag, but no amount of finagling, cajoling... etc will move it.

Re: Reorder features in assembly?

Esteemed Contributor
Esteemed Contributor

What Matt said.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200