Cancel
Showing results for 
Search instead for 
Did you mean: 

Reorient Drawing Views

I am new to Soild Edge and have a couple of drawing view questions:

 

1) Is there a way to reorient a drawing view "after" the view has been placed on the drawing? For instance, I want to flip from front view to back view or change from right side to left side.

 

2) I see it is possible to change the rotation angle of a drawing view but it does not reorient the projection views. Is there a way to rotate a view and have the other projection views change also?



David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
3 REPLIES 3

Re: Reorient Drawing Views

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi David:

 

The simple answer is - No, even if it sounds harsh.

This topic was discussed recently in this post and hopefully you will find answers to most of your queries there-in, especially the last answer #10 in that topic by @scott_lester.

 

~Tushar Suradkar

www.CADVertex.com

 

Re: Reorient Drawing Views

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have to take exception, Tushar, regarding number 1. Using PMI model views you can change the orientation of views. Discussed in this post:

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/How-to-extract-other-views-from-Iso...

 

pmiview.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Reorient Drawing Views

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

That message certainly missed me Bruce.

May be I will make a good tip-trick out of the post.

@Imics already has the video Smiley Happy

and that's the benefit of standing on the shoulders of giants Robot Very Happy

 

~Tushar