Repeat command.

Creator
Creator

In Autocad the space bar allows you to repeat last command.  Is there a function in Solid Edge that duplicates this?

3 REPLIES

Hi,   Unfortunately SE doesn't offer repeat last (1,2,3.....

Phenom
Phenom

Hi,

 

Unfortunately SE doesn't offer repeat last (1,2,3...) command what was used by user.

 

BR,

Imi

Imics
http://solidedgest.wordpress.com/

Re: Hi,   Unfortunately SE doesn't offer repeat last (1,2,3.....

Esteemed Contributor
Esteemed Contributor
Commands auto-repeat by default until you start another command (and Select is a command).


Ken

Production: ST10 MP3
Testing: SE 2019

Re: Hi,   Unfortunately SE doesn't offer repeat last (1,2,3.....

Phenom
Phenom
Ken,

Yes, you are right, but if you use Select command then there is no way to back the "real" last used command. Other softwares offer a short list about "last used commands" and you can choose from them... This is very useful.

BR,
Imics
http://solidedgest.wordpress.com/