Cancel
Showing results for 
Search instead for 
Did you mean: 

Repeating a Revolved Protusion

Creator
Creator

Hi,

 

First off thanks for taking your time to read my post.

I am using Solid Edge V20.

I have attached an image to make my problem clearer.

 

The part is comprised of two revolved parts. 

The first revolution is a complete revolution and is fine as such.

The second revolution is only over a distance of 6°. Now I want to repeat this revolution 29 additional times to make for 30 evenly spaced parts of 6° each. I have tried this with the pattern tool but I can't seem to be able to select a revolution as a feature?

 

Many thanks in advance,

 

Hendrik

 

4 REPLIES

Re: Repeating a Revolved Protusion

Phenom
Phenom

It seems to work fine in ST7. I have no way to test in V20, but there is no reason this should not work in V20 also. If you post the file I can try it, but you won't be able to open it once I save it.

 

I would note that your second revolved protrusion appears to be a closed profile and it does not need to be closed. You can use open profiles in SE. 

 

PatternRevolve.jpg

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Repeating a Revolved Protusion

Creator
Creator

Hi Bob,

 

Thanks for you response.

I have attached the file for the sake of testing.

 

Hendrik

Re: Repeating a Revolved Protusion

Phenom
Phenom

Are you using an academic license? I am unable to open the file.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Repeating a Revolved Protusion

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

I agree with the opinion to closed vs. opened profiles.

 

Here an open profile should be prefered.

 

And in my opinion I would go the other way round.

Create a full rotational cross section and then make one cutout.

Try to pattern this cutout.

And again use an open profile too.

 

Regards

Wolfgang 

 

 



regards
Wolfgang