04-05-2017 09:24 AM
Hello,
This is what I am trying to do but I cannot get the dimensions to remain attached:
1. Import step file into ST9, save as assembly (successful)
2. Create draft(s) (successful)
3. Import new step file of same geometry with changes (Same names for all assemblies and parts) [Successful]
4. Update draft(s) for file with the minor changes [Unsuccessful: all dimensions detach]
I have tried using 'Design Manager' with 'replace part' and also 'Edit links' in the draft document. Neither have been successful.
If there is a way of doing this simply so that it can be done every time I need to important an updated geometry that would be great please
04-05-2017 11:53 AM
Probably should ask this in the Solid Edge forum. This is targeted to the Free 2D product which does not include the 3D parts...
https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/bd-p/solid-edge-forum
04-05-2017 11:57 AM