Cancel
Showing results for 
Search instead for 
Did you mean: 

Replace part/Assembly in draft environment by family of part/Assembly

Pioneer
Pioneer

Hello Everyone,

 

I have a shaft which has number of family member. I am created a drawing of one member from family of parts.

 

I wants for replace this drawing with another family member.

Is it possible ? if yes then how?

3 REPLIES

Re: Replace part/Assembly in draft environment by family of part/Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Check out "Edit Links" available in the draft environment. I have it in my quick access toolbar but it's under the application button under "info".

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: Replace part/Assembly in draft environment by family of part/Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Harsh9592

 

 

You can do this with using the "Edit Links" function under Info of Solid Edge

20171026_2013.PNG

 

or what I would prefer is to use a  FOP table in that draft

220171026_2017.PNG

regards
Wolfgang

Betreff: Replace part/Assembly in draft environment by family of part/Assembly

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello @Harsh9592

 

Kindly mark all appropriate and helpful posts as "Accepted Solution"

Thanks.