Cancel
Showing results for 
Search instead for 
Did you mean: 

Replace parts or subassembly in assembly environment using excel link

Pioneer
Pioneer

Hello Everyone...

 

I have two parts.

1) shaft (have 2 or 3 family of parts)

2) Cylinder (have 2 or 3 family of parts)

 

I created family of assembly (named X & Y) using above two parts.

 

I created another Assembly using above family of assembly (suppose Using X member).

 

I wants to replace X member with Y member using Excel...

Is it possible ? if yes then how??

 

 

 

4 REPLIES

Betreff: Replace parts or subassembly in assembly environment using excel link

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Harsh9592

 

 

before answering allow me the questionn what Your intends are?

 

What will You change using Excel and what will be Your benefit doing so?

 

I - and this might be a very personal opinion only - I do not like to have Excel involed, as long as there is no good reason for it.

Especially if You can do it within the "Family" (what means Solid Edge)

 

So maybe the overall aspect can help to give You the better answers

 

Besides this, I'm also not a real friend of a real "Family of Assembly".

Alternate position, Yes this is OK, but a real familiy with different assemblies and - this is important - different document numbers and structures of BOM, this very soon will lead to a very bad performance.

At least this is what I have in mind.

 

But - and this is the good story, there are altenrative approaches and methods to use, which IMHO will lead to a better and easier result.

 

regards
Wolfgang

Betreff: Replace parts or subassembly in assembly environment using excel link

Pioneer
Pioneer

Thank You @hawcad

 

Excel driven family of parts/Assembly is useful when you have a large assembly & Assembly have multiple components & each components have multiple family member.

 

If we can link up all those family of parts/assembly with excel then it saved lot of time.

 

we can eliminate the process... select the component > replace Component > select required one components....

 

Hope You understand my query..

 

thank youSmiley Happy

 

 

 

Betreff: Replace parts or subassembly in assembly environment using excel link

Valued Contributor
Valued Contributor

I was about to post this same question, then i found someone has already asked it.  Is it possible to get excel to replace parts in an assembly?  I've seen people modify variable tables for part files with excel but I have never seen someone replace parts in an assembly with excel. 

Betreff: Replace parts or subassembly in assembly environment using excel link

Pioneer
Pioneer
Sorry i didn't find the solution...

If you find the solution then please share it on forum...thank you...