Cancel
Showing results for 
Search instead for 
Did you mean: 

#Request! Api for to create groups according to color and thicknesses

Pioneer
Pioneer

Hi.

 

Is there a way to convert a recorded macro in femap to an API code ?? I have below an API code to run in femap to create groups from color, but my code seems to be off as I am not the familiar with programming. Any suggestions or changes to the code will help as well as an API code to save what is within the graphics window to a jpeg. Please help.

 

Sub Main
Dim App As femap.model
Set App = feFemap()

Dim color_ As femap.color
Set color_ = App.feColor

Dim group_ As femap.Group

Dim colorOnSurf_set As femap.Set
Set colorOnSurf_set = App.feSet

While color_.Next 'go through all colors
If (color_.ID <> 1) And (color_.ID <> 9999)
App.feAppMessage(FCM_NORMAL, "Working on color :" & Str(color_.ID) &"=>" & " " & color_.title )

colorOnSurf_set.Clear
colorOnSurf_set.AddEntitiesOnSurf( -color_.ID, FT_SURFACE) ' collect surfaces in the set


Set group_ = App.feGroup
group_.title = color_.title
group_.SetAdd(FT_SURFACE, colorOnSurf_set.ID) ' add surfaces from the set
group_.Put(group_.NextEmptyID)
End If
End While
Wend
End Sub

3 REPLIES 3

Re: #Request! Api for to create groups according to color and thicknesses

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This is the Solid Edge Forum.  May have beeter luck in a FEMAP forum.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: #Request! Api for to create groups according to color and thicknesses

Pioneer
Pioneer
Hi. Thanks I thought it was all one forum. Smiley Happy

Re: #Request! Api for to create groups according to color and thicknesses

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Nope, that's why this one is called "Solid Edge Forum" Smiley LOL

 

Try this one: https://community.plm.automation.siemens.com/t5/Femap-Discussion-Forum/bd-p/femap-forum



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com