Cancel
Showing results for 
Search instead for 
Did you mean: 

Required a straight tapered & tapered cut in solid edge ST10

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Trying to generate a screw which is straight- tapered -straight in shape.

 

Tried using solid sweep but it is following a straight cross sestion only because of which steps are created.

 

Can anyone suggest how we can create a cut on the model.

 

Model is attached for your refrence.

 

Thanks in advance.

2 REPLIES

Re: Required a straight tapered & tapered cut in solid edge ST10

Valued Contributor
Valued Contributor

Well I guess (from the attached model) yout are trying to make a helical thread on the outer surface of the clindrical surface

 

So sweep is not the correct command to do this operation..

 

Rather use Helix

 

 

Untitled.png

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Let me know if you were able to perform the required action

 

Capture.JPG

 

 

 

 

 

 

 

 

Re: Required a straight tapered & tapered cut in solid edge ST10

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Shiv,

 

But when we used Helix cut the depth in tapered and straight does not match .

 

Requirement is we want to match the depth as well.

 

Thanks for the reply.