Cancel
Showing results for 
Search instead for 
Did you mean: 

Retrieve Dimensions Command

Pioneer
Pioneer

Is there a switch/option that turns the Retrieve Dimension command off/on? The reason I am asking is that I have used this command in the past but now when I select a view, using the command, nothing happens.

 

Thanks

 

Dave

4 REPLIES

Re: Retrieve Dimensions Command

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Start the command and look on the Command Bar.

Make sure you you are not in Remove Dimensions mode.

LMGi
www.TLMGi.com

Re: Retrieve Dimensions Command

Pioneer
Pioneer

Yes, I made sure that this options is not selected. I am sure if has worked in the past that I must have changed a setting somewhere else that I did not catch.

Re: Retrieve Dimensions Command

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As long as there are dimensions created in the model on planes that are parallel to the the drawing view and as long as you have the correct Retrieve options set, they should come in.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Retrieve Dimensions Command

Pioneer
Pioneer

Yeah, the dimensions are all there and it has worked fine up until MP2. Thanks for the input. I'll keep digging.