Cancel
Showing results for 
Search instead for 
Did you mean: 

Revolve For A Cylinder

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

With this revolve for a cylinder with a 30° angle.

I've noticed the angle is to sharp, What is needed to establish a gradual angle to be a 60°. I've tried a 15° angle to a 30° no good.

 

http://screencast.com/t/3PMv8XLG8I

 

Thanks 

Greg

2 REPLIES

Watching this video may help..... https://www.youtube.com...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Watching this video may help..... https://www.youtube.com/watch?v=LwYsAcjWRfE

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

I suspect it is because your axis of rotation is not on t...

Phenom
Phenom

I suspect it is because your axis of rotation is not on the same plane as the face being revolved.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.