Cancel
Showing results for 
Search instead for 
Did you mean: 

Ribbon not showing up, random crashes, etc...

Pioneer
Pioneer

This has been going on now for a while, and I thought buying a new graphics card would help.  It hasn't.  Whenever I open um ST9 the ribbon is blank my views, blocks, and more will vanish upon zoomin in and out.  Everything gets really glitchy, and when i try to close the file the whole thing crashes and I get a windows warning saying "Solid Edge has stopped working".  

 

I made a video so you can see what I'm talking about.

 

Any ideas?

4 REPLIES

Re: Ribbon not showing up, random crashes, etc...

Legend
Legend

Hello,

can you disconnect all usb devices besides the mouse. I had something similar with my mobile connected via usb.

Greetings from Germany
Christian Kunkel
https://c-k-m.info

Re: Ribbon not showing up, random crashes, etc...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try this:

Close Solid Edge
Stay logged on as your normal user (not administrator or something)

Open Regedit.exe, a Windows tool to edit the Registry (Start, Programs, Command Promt. This will start a DOS-promt. Type [regedit] and press Enter). This can depend on what OS you're running.
Browse to HKEY_CURRENT_USER\Software\Unigraphic Solutions\Solid Edge\[Version in use]\[Application]\Toolbars
where [Version in use] is the version of Solid Edge you are using and [Application] is Assembly, Part etc. of which the toolbars have disappeared
Delete the 'directory' Toolbars.
When starting Solid Edge, the default toolbars should reappear.
Note: Editing your registry can make your computer unusable. If you are not comfortable with this, ask for help from the CAD manager.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Ribbon not showing up, random crashes, etc...

Pioneer
Pioneer

Holy crap it worked!  Thank you so much.  Why the heck would this happen?

Re: Ribbon not showing up, random crashes, etc...

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
I've logged this as an issue with the Siemens GTAC team, it's currently in progress for an emergency fix...

The issue appears to be windows 10 specific and associated with USB hardware; phones in particular
Kind Regards,
Jack Stark

Majenta PLM - Siemens Platinum Business Partner
http://majentaplm.com/