Cancel
Showing results for 
Search instead for 
Did you mean: 

Right and a Left Twist

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Good Afternoon Everyone,

With this doc. I would like to learn a right hand as well as a left hand twist. As you can see there are numerous curves. 

Included are the video off the Solid Edge as well as mine.

 

Solid Edge ST4 Surfacing Helix Demo

http://screencast.com/t/g2Zbu4sboq

 

Thank You All

Greg

1 REPLY

Not sure what you are attempting to do since you already...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not sure what you are attempting to do since you already have a solid created.  To create a sweep you need a path which is selected first, then a cross section sketch that is selected second.  After both are defined, you can then edit the options to add twist.

 

http://www.youtube.com/watch?v=CyYUocUHXf0&feature=youtube_gdata



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com