Cancel
Showing results for 
Search instead for 
Did you mean: 

Roll back to MP3

Honored Contributor
Honored Contributor

Is there an easy way to roll back from ST9 MP4 to MP3.

 

I recently upgraded to MP4 and then I started crashing frequently. 

 

The most common action causing the crash is changing the gage of a sheet metal part.

 

What is the path of least resistance to roll back to MP3?

1 REPLY 1

Re: Roll back to MP3

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Use the "Programs and Features" command and select the entry in the upper left to Show Installed Updates.  Find Solid Edge ST9 in the list and double click to uninstall.  It will roll back to the last installed update.

2017-01-31_15-50-29.png



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com