Cancel
Showing results for 
Search instead for 
Did you mean: 

Rotate

Pioneer
Pioneer

Hi,

 

i am having problems on the rotate command on the mouse, as i have no rotate red dot to get a fixed point to rotate from,

 

any ideas

 

paul,

9 REPLIES 9

Re: Rotate

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi:

 

First click with the middle mouse button or the scroll wheel and pick a coner/vertex to get the red dot to rotate about.

 

~Tushar

 

Re: Rotate

Pioneer
Pioneer

Tried that one still no good,

i have also tried clicking on the rotate command button, but it just gives me a axis to rotate around. with no red dot.

 

Thanks

Re: Rotate

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

What is the Solid Edge version ?

 

Re: Rotate

Pioneer
Pioneer

Hi,

 

i am using ST6.

 

Thanks

Re: Rotate

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Great. I am on ST 6 as well.

7 days time makes a thread on this buzzing forum a really old topic but I could not simply let this get off my mind.

After playing more with the middle-mouse rotate, I noticed it is not necessary to first middle-click to get the red/pink dot to rotate about nor pick or specify it on model geometry and then proceed to actually rotate.

 

This can all happen in one 'Go'.

Might already be known to many and also somewhere deep in the help files but what I found was I could keep the middle-button pressed a 'bit longer' and Solid Edge automatically 'grabs' the pink dot following which I could continue to rotate the model.

 

So all I did was without starting any command and just by making sure that the mouse cursor 'is over some geometry' like a face, edge or a vertex and 'not in empty space', pressed the middle-mouse-button and kept it pressed for a bit while to create and grabs the red dot in one shot and continued to rotate the model.

 

Without any geometry under the cursor, the model would rotate unpredictably.

 

Not sure if this solved your problem or if it is already solved but give it a try and update here if possible.

 

Below is a video: no geometry under cursor means un-predicatable rotatation.

And with geometry under cursor, the red-dot appears automatically, just keep the middle-button pressed a 'little longer'.

 

Re: Rotate

Pioneer
Pioneer

I shall give it a try, first thing monday morning.

 

 

Re: Rotate

Experimenter
Experimenter

Had the same problem for many years (ST series) that Renderer option removed the "ball" opportunity. 

 

Advanced and Direct 3D rotate by the model center, while Basic allows the ball aka View Center. 

 

No matter how long I wait or hold or pray for the ball, its not there. 

 

The frustration of NOT being able to use the full power of my GPU (D3D) AND the red ball aka View Center

Re: Rotate

Phenom
Phenom

To add to this you can select a point to rotate about using the Rotate command on the View Tab. 

 

Basically you select the rotate command and then move your mouse to a vertex on the model and click. The rotate center then moves to that vertex so you can rotate about the vertex or select and axis and rotate.

 

See attached video.

 

(view in My Videos)

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Rotate

Experimenter
Experimenter

Yes, you can use that

 

Problem is: why can SE place a rotate center where the mouse pointer is in one rendering mode, but not in others? And I have used all possible combinations to make this feature happen in different rendering modes: zoom in, hold time, different settings etc.

 

How much time can you save, when the rotate center is automatically placed, where the mousepointer is on a visible surface? It seems like a real time-saver... and now that I have said it, it will be an Apple-style accessory add-on. $5.99 maybe?