Cancel
Showing results for 
Search instead for 
Did you mean: 

SE Assembly

Experimenter
Experimenter

Is there a way I can change a PART color in the Assembly environment? For instance, can the color palat icon be loaded onto the assembly task bar and then address a part from the expanded tree?

5 REPLIES 5

Re: SE Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Click on a part and select "face overrides" in the "view/style" menu.

 

faceoverride.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: SE Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Make sure you have individual part styles turned on.

 

faceoverride2.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: SE Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes, as @bshand says........just also be aware, in assembly, it colors the entire part, regardless of face styles already set on that part, like threads for instance.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: SE Assembly

Experimenter
Experimenter

Thank you for the three tips.

Re: SE Assembly

Experimenter
Experimenter

Thanks Bruce.