10-16-2017 05:17 AM
SE CID Utility error when I get Composite ID from Windowns 10 Home.
Thank you.
Solved! Go to Solution.
10-16-2017 05:33 AM
This is nothing to do with your operating system or computer type per se. This is an error telling that you are missing the msvcr100.dll file.
At best you are just missing the Visual C++ runtime which can be resolved by downloading and installing the Runtime. At worst, you have some serious issues with your system that will take major investigating and debugging.
See this great post on resolving msvcr100.dll error:
https://www.lifewire.com/how-to-fix-msvcr100-dll-not-found-or-missing-errors-2623799
10-16-2017 06:06 AM
HI @Famer
I woul dlike to ask a quite different question:
"Will a computer with a I3 processor with 2.3 GHz and 4GB of memory powerfull enough to run Solid Edge?"
I rember to had a similar computer a couple of weeks ago, where the login procedure, etc. a took to long time and starting Solid Edge was possible but not using it.
Another issue might be the graphics card.
10-16-2017 06:07 AM
HI
OK, nVidia Gforce will handle Solid Edge
Take care about the correct driver