Cancel
Showing results for 
Search instead for 
Did you mean: 

SE PDF printing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,


I have to start an old issue again.

 

A user claims that when printing a SE draft to PDF, the page (paper size) in PDF is NOT exactly what was definend in draft.

 

No laugher now:

example: paper is 420x297 (Yes, this is an A3) and pdf will be 420.16 x 297.04

 

OK, this is just a part of a mm but it still is not exact what it should be.

Using a different PDF printer will result in a proper page size.

 

 

Can anybody confirm thios as a ST9 "change" (bug) or is there a hidden setting some where?

 

Thanks in advance

 

regards
Wolfgang
4 REPLIES 4

Re: SE PDF printing

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Just as a reference.

When I do Save As PDF from ST9 MP2 and then open the PDF in Adobe Reader XI it measures exact.

I measured the boarder of 574mm.

Jason T.

LMGi
www.TLMGi.com

Re: SE PDF printing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JasonTitcomb

 

 

just the default setting for export as PDF, nothing secret?

 

Can You upload the pdf  and Your draft please?

 

 

 

 

regards
Wolfgang

Re: SE PDF printing

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Now I get a small error on some. .01mm

No settings have been changed in the printer.

LMGi
www.TLMGi.com

Re: SE PDF printing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JasonTitcomb

 

it is just the same as here.

Not only the measurements are slightly different but also the paper size.

 

OK, it's just 0,1 mm but our users complained it.

 

Your pdf properties also show 594.1 x 420.2 mm for this A2

 

 

 

 

regards
Wolfgang