Cancel
Showing results for 
Search instead for 
Did you mean: 

SE V20 Academic: constrain motion in assembly

Experimenter
Experimenter

When using Move to drag or rotate a part in an assembly.. i.e a hydraulic cylinder piston; how to avoid pulling the piston out of the cylinder ?

Maybe a collision sensor at each end, but are there any other / better way ?

1 REPLY

Re: SE V20 Academic: constrain motion in assembly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I do not believe that V20 had the Range Offset for the Mate command or the ability to constrain to a path. These came in later versions. V20 is now 7 years old.

One thing that you can do is set the Analysis Options to "Stop motion when collision occurs"

c1.JPG

and then select "Detect Collisions" and  in the command ribbon.

c2.JPG

Whilst this is not as precise as later methods it may suffice.

Cheers

Mark