Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

SE draft: extracting custom variables from part file to custom table

Valued Contributor
Valued Contributor

I have made custom table and I want to extract custom file properties from part file to this table.

How this is done?

 

I tryed making a custom table that has 3 colums value name, value unit and value.

value name and unit are just text, but value I want to extract from part file, like this: %{Module/CP|R1}.

But it shows this as a text, with callout it works well.

 

what Im doing wrong

1 REPLY 1

Re: SE draft: extracting custom variables from part file to custom table

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Table command does not support property text as data.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com