Cancel
Showing results for 
Search instead for 
Did you mean: 

SE2019 - MP07 available since May 8th

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi edgers,


surprisingly I just have seen, that there is the MP07 for SE2019 available in GTAC downloads.

And that since May 8th

 

Have I overseen anything, or was there no information about?

 

 

regards
Wolfgang
11 REPLIES 11

Re: SE2019 - MP07 available since May 8th

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad Actually it just posted today.  The date shown is the creation date and it has been in testing since it was created till today.  It was not there this morning, and Support usually posts to the Forum once it has fully uploaded to all the download servers.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: SE2019 - MP07 available since May 8th

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG 

 

 

 

thanks a lot, I really thought that I have missed something on my old days!

 

 

regards
Wolfgang

Re: SE2019 - MP07 available since May 8th

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So is this going to be officially announced? BTW there are no executables in the Insight server folder so perhaps it isn't ready for prime time.

Go with MP6 as the latest for now?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: SE2019 - MP07 available since May 8th

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@bshand You still using Insight... What's your "goto" plan?



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: SE2019 - MP07 available since May 8th

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@bshand Looks like Insight patch README's have posted, so appears the bits are in process...



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: SE2019 - MP07 available since May 8th

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@KennyG, we haven't settled that yet. Not anxious to go with TC. Considering DBSolidedge.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: SE2019 - MP07 available since May 8th

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@KennyG wrote:

@bshand Looks like Insight patch README's have posted, so appears the bits are in process...


Somewhat interestingly there generally aren't readmes in that folder in released MPs.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: SE2019 - MP07 available since May 8th

Siemens Legend Siemens Legend
Siemens Legend

@hawcad The MP7 executables were in fact created on 8-May-19 as part of the build process. MP7 was then made available for internal testing and validation. The validation process finished up on Friday 17-May-19. The readme file and announcements were then updated to reflect the PRs that were verified as fixed and MP7 was posted on Monday 20-May-19. I would always advise waiting on the MP announcement before downloading as it is possible the download servers have not yet had a chance to fully sync, which could result in you getting a partial download. 

 

 

Regards,
Fred White
Siemens PLM Software

Re: SE2019 - MP07 available since May 8th

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JFred 

 

 

 

thanks for that info.

 

And could it be, that the problem mentioned in the other post is coming from a "to early download"?

 

 

regards
Wolfgang