Cancel
Showing results for 
Search instead for 
Did you mean: 

SE6 can not be registered - SELicense.dat does not exist

Experimenter
Experimenter

Hello there,

 

I just tried to register my 32bit version of SE6.

Unfortunately there is an error message following the procedure.

It seems that the SELicense.dat file does not exist.

 

I tried to install the software unter Windows 10 64bit to test it for use on out 32bit student machines.

 

Please help

 

Alex

 

 

 

2 REPLIES

Re: SE6 can not be registered - SELicense.dat does not exist

Siemens Legend Siemens Legend
Siemens Legend

Hi Alex

 

Sorry to hear that you are having problems registering your product.

 

Could you please email a screenshot of the License Utility where you entered your license key?

 

Thanks

Melanie

melanie.baeske@siemens.com

Re: SE6 can not be registered - SELicense.dat does not exist

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Alex,

 

Two things come to mind.....[further to the expertise that @Melanie_Baeske will be able to offer]

 

  1. Are these new PC's with only ever having Windows 10 installed, or are they upgraded units from Win7, or 8[.1]?  [as you may need to install Microsoft .NET Framwork 3.5 also, if Solid Edge has never been on these before]
  2. Seeing as the new PC's have 64bit operating system....could you not just upgrade these to the latest version...ST8? [this should load without issue]
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000