Cancel
Showing results for 
Search instead for 
Did you mean: 

SEAdmin

Valued Contributor
Valued Contributor

When I try to open the SEAdmin.exe file I get a dialog box that pops up saying: "Unable to read the configuration file.  Open a different configuration file or create a new one."  This exe file was copied from the DVD and put into the C:\program file\Solid Edge ST6\Programs folder per the instructions in the Help menu.

 

What do I have to do to get this to work?

3 REPLIES

Re: SEAdmin

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Does the program  open though and give you the file and help menus?

Maybe you need to open an options.xml file since that is what seadmin is for...

 

Edit: reading the help it refers to the options.xml file as a "configuration" file.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: SEAdmin

Valued Contributor
Valued Contributor

I got it to work by opening up an older options.xml file and then I editted that and save it out as options.xml.


@bshand wrote:

Does the program  open though and give you the file and help menus?

Maybe you need to open an options.xml file since that is what seadmin is for...


 

Re: SEAdmin

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Makes sense. Good.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200