Cancel
Showing results for 
Search instead for 
Did you mean: 

SEEC Create Package

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

I cought in promotion video (ST9 What's new - Enhanced Teamcenter integration for solid edge) the function Create Package to download zipped data. I have installed latest SEST9 MP4 (109.00.04.005) but I can not find this function in Teamcenter menu. Is this function something special (license) or just need to turn it on?

3 REPLIES

Re: SEEC Create Package

Gears Phenom Gears Phenom
Gears Phenom

IIRC  that is within Design Manager...???

 

Not in a position to test / check at the moment.

 

take a look there.

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7
Highlighted

Re: SEEC Create Package

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

i reply myself. As usually: "Read the manual first"

Note: This command is enabled using the Teamcenter preference SEEC_Enable_Create_Package

 

Re: SEEC Create Package

FWIW, the actual Teamcenter Preference name is SEEC_Enable_CreatePackage, not SEEC_Enable_Create_Package.

 

Refer to the SEECAdminGuide.pdf file delivered in the .\Solid Edge ST9\Program\ResDLLs\0009 folder.

 

Regards,

 

Kevin