Cancel
Showing results for 
Search instead for 
Did you mean: 

SEEC Structure Editor on ST9

Phenom
Phenom

Has anyone used Structure Editor on SE ST9 & Teamcenter 11?

 

Since upgrading from ST7 and TC9 recently, structure editor is unuseable on anything but small assemblies. I can't even get it to open medium asms with few links.

 

Just wondering if it is a common issue, or something in our setup.

5 REPLIES 5

Re: SEEC Structure Editor on ST9

Siemens Phenom Siemens Phenom
Siemens Phenom

There are some Structure Editor fixes in MP1 and MP2 so you definitely need to be on MP2 at this point regardless.  There is specifically a fix in MP2 related to Structure Editor and linked files but this may or may not be the same issue that you are experiencing. 

Re: SEEC Structure Editor on ST9

Phenom
Phenom

Thanks Dave, I'm on MP2 already unfortunately. Actually Siemens gave us a workaround registry fix for the linked file bug fixed in MP2.

 

I left structure editor open overnight and it was able to open a medium assembly (actually smallish compared to some we do), but now every change to any cell in the window is taking about half an hour to process - not big changes with links, just the description of the dataset for example.

 

I was just wondering if people were using StrEd sucessfully with ST9 and it's just us, or is it a general issue?

Re: SEEC Structure Editor on ST9

Siemens Phenom Siemens Phenom
Siemens Phenom

To be honest, not seeing any reports of such behaviour from other SEEC customers.

Re: SEEC Structure Editor on ST9

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi all,

 

I have the same Softwareversions in use.

 

I just tried to open an assembly in Structure Editor, works fine, alse "Save As All" reacts like i am used to it before.

 

Did you change configuration during the upgrade from ST7?

 

Re: SEEC Structure Editor on ST9

Phenom
Phenom

Thanks @c_weber, at least I know it must be something in our setup. Our configuration shouldn't have changed during the update but obviously something is wrong. I'll have to log it with our VAR.