Cancel
Showing results for 
Search instead for 
Did you mean: 

SEStatus change on managed file

Valued Contributor
Valued Contributor

I am setting up a managed system to use the life cycle with insight. I have moved a file from released back to prelease. i do not want to revisie the file at this time. The SEstatus still says released. how do i change it while it is read only within property manager?

Nathan M. Gardner

https://www.etsy.com/people/NathanMGardner

Be sure to check out my work!!
Made in Maine Wood Carvings

1 REPLY

You cannot, however you can edit the property in SharePoi...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You cannot, however you can edit the property in SharePoint to "Available" and then open it and it will synchronize the property to the file so that it now witeable and Available.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com