Cancel
Showing results for 
Search instead for 
Did you mean: 

SEU session on Reverse Engineering

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Thursday , October 28

 

11:15 AM  -  12:00 PM
Reverse Engineering in Solid Edge  (White River A)
Come learn about Reverse Engineering, a new Solid Edge beta-stage add-in that provides tools to convert STL mesh data to a Solid Edge part model. See how to import an STL file, repair STL mesh, identify shapes, extract surfaces, create a construction body, and convert it to a design body that is ready for editing and use in Solid Edge.  At the end of the session, you will have an opportunity to help direct future development of these tools.
Speakers:

 

http://www.cvent.com/events/solid-edge-university-2016/agenda-d8e7e3e4756540c895bcc947169824ea.aspx

4 REPLIES 4

Betreff: Test

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Sandeep,



this looks "GREAT" !

Can You tell us a little bit more about this modul/addon?

 

When will it be available, what's about cost, and so on.

 

Thanks a lot for something we was expecting a long time!

 

 

 

regards
Wolfgang

Betreff: Test

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

That is a ST 10 'sneak' peek

Right Sandeep ?

Betreff: Test

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Yes thats right !

Betreff: Test

Genius
Genius

Hi Sandeep,

 

This is really great news!

Is it the Siemens NX add-in fitted for SE or is it a third party add-in or a complete new add-in ?

I hope it's not the second one because if so it will be released at the competition also.

Anyway I suppose you cannot share any video so I have to wait and see what's heading to us.

 

But still it's great news anyway !! And hope it's also affordable....

 

Dirk Rutten

Solid Edge ST6 user !!!!