Cancel
Showing results for 
Search instead for 
Did you mean: 

SOLID EDGE DRAFTING BACKGROUNDS

Pioneer
Pioneer

HI

 

I have never understood why it is only 4 drafting backgrounds in SE
And just wide backgrounds.
I understand that many people want to create their own templates, but for those of us who do not need our own custom backgrouns, it would have been nice if there had been a larger selection default, maybe for all default sheet size.
As some other cad software has.
Does anyone know if there are any ready-made drafting background packages any place we can download.
Or does anyone want to share their background package?

17 REPLIES 17

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@centernorway 

 

 

 

so I can not understand this "request" or complaint.

 

I must say, that I do not know any user or customer who does not have adapt the draft templates to his requirements.

And, if You - as You mentioned - do not need any adaption, just use the DIN template of Solid Edge.

There will be all paper sizes from A4 to A0 and A4 in both orientations too!

 

No need for any additonal efforts or work to do.

 

 

regards
Wolfgang

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Pioneer
Pioneer

You dont understand my question.

Are you living in her Wolfgang, you coment all posts in this forum Smiley Happy

But my question is about that It is only 4 wide titleblock backgrouns default in SE.

Re: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @centernorway,

 

Seeing as almost EVERY company has their own version [same, but different] of a Draft template layout, only base is installed by default.....and seemingly the background sheets have always only ever been delivered as landscape.

It really isn't that big of a deal to create your own, based on that and rename them to suit your company. I have them for the four business sectors of our company, and focused mine to only be on A3 sheet size, in both Landscape [the default] & Portrait layouts.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @centernorway 

 

 

and my answer was, that if You use the DIN template then You will found even 7 backgrounds.

A0 to A4 (both landscape as  well as portrait) and a BOM background.

 

The templates just are files, so You can copy it to Your template folder, YOu can rename it as You like and You also can change the drafting standard accordingly.

 

I do not see, where the problem might be.

 

And no, I'm not living here!

Smiley Wink

regards
Wolfgang

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And here just for showing it:

 

20190213_1942.png

Edit:

And also the DIN template IMHO has the better proeprty text information already in use.

So from there YOu will be able to adapt it in a much easier way as e.g. using the ISO template.

 

 

regards
Wolfgang

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thanks @hawcad , I've looked at DIN [and others] templates and only find landscape backgrounds. I have favoured the ISO templates, since forever ago, and quite stubbornly, have kept the same base template over the years of releases.

 

Sorry Wolfgang, but I have to disagree, you really DO live here! Robot LOL This forum is your 2nd FAMILY home. Robot wink

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad is the ubermensch of the SE forum.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Spot on @bshand,

 

"Oh ja, er ist einfach so".

Sorry for my crude attempt to recall any of my German learning from school days. Robot Embarassed

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Pioneer
Pioneer

Ok

Thank for tips everyone.

Looks like I have to draw my own titles block backgrounds then.
My opinion is that when you buy software for xxxxxxxxxxxxxxx dollars, there should be tons of bakgounds to Smiley Happy

I think I should developed the best cad software if I could, and if I had the skils an money.

It is not any perfect cad software out there yet Smiley Happy