Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Phenom Gears Phenom
Gears Phenom

@centernorway  - I disagree with this request. There is no way that Siemens can make every user happy when delivering background templates. Plus, as others stated here, 99% of companies will have their own custom templates that will be used. I've yet to work for a company that didn't have their own backgrounds.

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Pioneer
Pioneer

I challenge the community Smiley Happy
What if we make a library where everyone shares their drawing templates / backgrounds and title blocks.
Who covers everything, catalog drawings, production drawings and so on?

A library where you can quickly find what you need.

And with file types you can import to all cad software.

What do you think about that?

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I personally am underwhelmed. In all my years of CAD use across many types I've probably spent about 0.001% worrying about drawing formats. And I can't think of many occasions where having more generic or more custom formats from other companies would have helped in any way. It always required a little customization which usually involved basically imitating, for the most part, the existing legacy formats which the company already had.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Legend
Legend

I agree, every company must have their own background formatted to what they prefer. How and where their company name/logo/address might reside is probably the biggest difference. I don't know anyone that would use the standard backgrounds that just say SOLID EDGE.

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand 

 

 


@bshand  schrieb:

@hawcad is the ubermensch of the SE forum.


is this to see positive?

And no, I'm just an "Edgeling"

 

Smiley Wink

 

regards
Wolfgang

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @centernorway 

 

 

again I must disagree to that 

 


@centernorway  schrieb:

Ok

Thank for tips everyone.

Looks like I have to draw my own titles block backgrounds then.
My opinion is that when you buy software for xxxxxxxxxxxxxxx dollars, there should be tons of bakgounds to Smiley Happy

I think I should developed the best cad software if I could, and if I had the skils an money.

It is not any perfect cad software out there yet Smiley Happy


 

 

I would like to see my invested money better spended as for creating tons of backgrounds, nobody ever will use.

Especially as there are available enough already.

To create Your own favourites and template will take a maximum of half an hour.

This - our - money could be used better!

Sorry!

 

regards
Wolfgang

Betreff: SOLID EDGE DRAFTING BACKGROUNDS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @SeanCresswell 

 

 

great! I never had thought, that people in New Zealand are learning German at school.

 

And no, besides living here I have a flat at the German CAD.DE Solid Edge forum Smiley WinkSmiley Very HappySmiley Wink

regards
Wolfgang

Re: SOLID EDGE DRAFTING BACKGROUNDS

Genius
Genius

A Tip!

Use Google and search for "dwg templates".

Just copy and  paste into a new SE draft template.

 

 

 

Solid Edge 2019