Cancel
Showing results for 
Search instead for 
Did you mean: 

[SOLVED] ST9 MP9 --> Fast search still broken?

Valued Contributor
Valued Contributor

In the past I installed MP8 on Solid Edge ST9, but I had to rollback to MP7 to have Fast Search working again.

 

Now I have installed MP9 but it has the same misfunction of MP8: fast search does not work and SE properties are not shown in windows explorer.

 

Any suggestion?

 

 

____________________________
http://www.stimarchetti.it
Design of automation
11 REPLIES

Re: ST9 MP9 --> Fast search still broken?

Valued Contributor
Valued Contributor

it seems that Windows does not allow me to uninstall MP9, any suggestion for this?

 

____________________________
http://www.stimarchetti.it
Design of automation
Highlighted

Re: ST9 MP9 --> Fast search still broken?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alessandro

 

 

 

You have turned on the update packages for the programs?

 

 

And I think "Fast Search" is not working correctling due to MP9 but probably due to a Microsoft Update.

 

Go through the "Obsticles of Fast Search" (see aother post) and check wether or not the SEPropertyHandler.dll is registered correctly

 

This happens very often due to operating system issues rather more than SE MPs

 

 

 

regards
Wolfgang

Re: ST9 MP9 --> Fast search still broken?

Valued Contributor
Valued Contributor

I already followed that article when I installed MP8 without solving the problem: actually the issue was related to the MP itself, and it was enough to rollback to MP7 to solve it, without any other operation.

 

What do you mean to turn on the update package? I was trying the same exact procedure that I followed when I unistalled MP8.

 

BTW, I think that if Solid Edge designers decide to base a so important function on a so weak Windows feature, thay are to blame too, imho.

____________________________
http://www.stimarchetti.it
Design of automation

Re: ST9 MP9 --> Fast search still broken?

Community Manager Community Manager
Community Manager

@Alessandro

I discussed this thread with development and GTAC today.  We are not aware of any problem with Fast Search in ST9 MP9.  The reported ST9 MP8 Fast Search issue was fixed and verified as fixed in ST9 MP9.

 

Please contact your partner to report this issue, so we can work to get this resolved for you.

 

Regards,

Laura

Solid Edge Release Manager.

Re: ST9 MP9 --> Fast search still broken?

Valued Contributor
Valued Contributor
After these two operations:

1) Install Fast-Search MP9 on the file server
2) re-register SEPropertyHandler.dll

now it works again (I guess the #2 was the good one).

Thanks to all.
____________________________
http://www.stimarchetti.it
Design of automation

Re: ST9 MP9 --> Fast search still broken?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Alessandro

 

 

 

as I thought and mentioned it:

 

"Again it was the registration of SEPropertyHandler.dll"

 

This is the most often happend issue in connection with the FastSearch

 

Need urgently repaired!

 

regards
Wolfgang

Re: ST9 MP9 --> Fast search still broken?

Valued Contributor
Valued Contributor

I have to thank you for the right suggestion. I was sure that this "re-registering" was already included in the MP script.

____________________________
http://www.stimarchetti.it
Design of automation

Re: ST9 MP9 --> Fast search still broken?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We too have seen this issue and have had to create a self installed patch for our users to register this when it occurs. Definitely needs fixed!



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST9 MP9 --> Fast search still broken?

Community Manager Community Manager
Community Manager

We escalated to development.  We'll take a look.

LKW