Cancel
Showing results for 
Search instead for 
Did you mean: 

ST 8 keypoint curve

Experimenter
Experimenter

In ST 7 the length of a keypoint curve could be fixed. In ST 8 is it possible to set a minimum radius for the curve ?

 

Brian

Brian White
Cascade Corporation
4 REPLIES

Re: ST 8 keypoint curve

Community Manager Community Manager
Community Manager

The standard keypoint curve does not support minimum radius. This IS suppored by the Wire Harness optional Solid Edge module. 

Dan Staples
Director, Solid Edge Product Development

Re: ST 8 keypoint curve

MLombard
Retired

That would make a great enhancement request, though!

Retired Community Manager for Solid Edge. This account is no longer active.

Re: ST 8 keypoint curve

I would love to see this added to XpresRoute. We model a lot of hydraulic flex hoses and a minimum radius is critical.

Regards,
Theodore
Kind regards,
Theodore Turner

Re: ST 8 keypoint curve

Experimenter
Experimenter

We are also using the keypoint curve to model hydraulic hoses.

The hose as a part file is created in the assembly using inter part copy of the hose fitting faces. This gives us the end points and the hose is shaped as required. The fittings are suppressed in the occurrance properties and the hose is defined by a common parts drawing.

The hose minimum radius is available in NX so it should be easy to add this feature to SE.

Brian White
Cascade Corporation