ST 8 stops working - Facebook Pane issue

Pioneer
Pioneer

Whenever the facebook pane is clicked ST8 stops working. It happens in all environment and with all files. 

However I do not need to access the facebook but if the pane is clicked by mistake, the software gets hanged and I have to forcefully close it from tast manager. All my unsaved data gets lost. 

 

Can anyone help me on this issue. Please refer the attached video. 

Diabling\Removing the facebook pane would also help. 

5 REPLIES

Re: ST 8 stops working - Facebook Pane issue

Phenom
Phenom

STOP using FaceBook... I have no idea why companies such a Siemens even uses FB at all.

 

Maybe I'm too old but all the STUPID Social Media is a waste of time.

 

Old Bob

Re: ST 8 stops working - Facebook Pane issue

Esteemed Contributor
Esteemed Contributor

Ditto what Bob said. Also just delete the FB link on that menu. Which might be a catch-22 if you can't expand the FB item and click the X in the upper right corner. Does it crash if you have nothing opened and open the FB in that menu?

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: ST 8 stops working - Facebook Pane issue

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: ST 8 stops working - Facebook Pane issue

Pioneer
Pioneer

I tried the workaround but didn't help. Aren't there any ways to disable the pane permanenty? 

Re: ST 8 stops working - Facebook Pane issue

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

It works for me fine. this is the first time i looked at it. a few good stuff in there