11-27-2017 12:33 PM
How can I add tolerance in ST10 to X and Y columns as I did in ST9?
ST9:
ST10:
No options for tolerance and no chance to hide the units
11-28-2017 04:04 AM
Hi,
You can edit hole table text in ST10 too. To hide unit you have to use /NU format code. To add tolerance you have to use format code and overwrite cells.
Here is a video:
BR,
11-28-2017 04:35 AM
Hi Imics,
Thanks for the solution to my problems with hole table.
Could you advise where to find a complete list of format codes?
BR
11-28-2017 04:43 AM
HI @MICROMECSRL
just click the Format button for every call out text.
This should show You all available format codes and YOu also can set them graphically.
11-28-2017 04:47 AM
11-28-2017 05:30 AM
It really is time that the tolerance could be included in the hole definition with the ability to bring that through into the drawing.
11-28-2017 06:36 AM
Hi @beachcomber
absoluteley correct.
Tolerance should be a value defined in 3d part document with the hole feature, and should be able to be retrieved into draft.
And this should be possible without any additonal setting, option, text, callout, etc.
Simply a button: "Show Tolerance!"
11-28-2017 09:27 AM
beachcomber wrote:It really is time that the tolerance could be included in the hole definition with the ability to bring that through into the drawing.
Yeah! Wow is that process ugly.
11-28-2017 09:30 AM
11-29-2017 09:00 AM
@beachcomberI agree with you, but we have already discussed about this...
BR,