Cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 MP1 LIST?

Valued Contributor
Valued Contributor

ST10 Mp1 List?
Here is the list.

ss1.png
I am just a local user. What should I install?

 

------------------------------------------------------------

Previously, MPs appeared in the update list on the control panel.
You can roll back if you want.


Self-test is a basic thing, please deploy quickly.

------------------------------------------------------------

 

2 REPLIES 2

Re: ST10 MP1 LIST?

Gears Phenom Gears Phenom
Gears Phenom

ST10 MP1 is not available yet

 

There will be a proper folder when ready, something like:

 

ST10 / Maintenance Packs / MP01 / Solid_Edge_MSI_MP1.exe

Betreff: ST10 MP1 LIST?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

You have to install none of them, when You are not using them.

 

But AFAIK thee will be no differences between Data Management tools in use for installations and - so I thibnk - for MPs too

 

 

The better question might be, where do You have this list from?

 

regards
Wolfgang