Cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 MP8 multibody modeling faliure

Pioneer
Pioneer

Hello Edgers,

 

Yesterday updated to MP8 to solve the step files problem, but i noticed a drop in performance on recalculating the features and sometimes doesn't shows  features even if I click on "recompute", and fails to create a solid body after the first feature. is anyone else experimenting the same?

 

Sketch.png

 

Josue

1 REPLY

Re: ST10 MP8 multibody modeling faliure

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Maybe if you toggle from construction bodies to solid bodies?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200